Armstrong In The Media

Armstrong Fluid Technology

Recent Posts

End suction pump

Posted by Armstrong Fluid Technology on Apr 24, 2017, 7:54:56 AM

As seen on csemag.com – April 13, 2017

The Design Envelope 4200 H split-coupled horizontal end suction pump is designed to adjust output to match the exact needs of an HVAC system in response to changes in system flow.

Read More

Topics: Uncategorized

Hydraulic Institute to bring Pump Systems Optimization Course to Canada

Posted by Armstrong Fluid Technology on Apr 17, 2017, 9:33:55 AM

As seen on mromagazine.com – March 29, 2017

Parsippany, NJ – For the past twenty-one years, the Canadian Institute for Energy Training (CIET) has specialized in high quality energy management and energy efficiency training and has trained over 7,000 professionals. The Hydraulic Institute (HI) is pleased to announce their partnership with CIET by adding their Pump System Optimization (PSO) course to CIET’s expanding training catalog.

Read More

Topics: In The Media

Armstrong’s New ‘Pump Manager’ Extends Performance Management Service Solutions

Posted by Armstrong Fluid Technology on Apr 7, 2017, 6:43:20 AM

As seen on empoweringpumps.com – March 23, 2017

Online Service Provides Sustained Performance, Enhanced Reliability

 

As a key component of its recently announced ‘next level of innovation in pumping solutions for enhanced building performance management’, Armstrong Fluid Technology has introduced Pump Manager.

Pump Manager is a web-based service that leverages the embedded intelligence and connectivity available through its technologically advanced new line of Design Envelope pumps to provide sustained performance and significantly enhanced reliability.

Read More

Topics: In The Media, Pump Manager

Living Up to LEED

Posted by Armstrong Fluid Technology on Apr 7, 2017, 5:51:13 AM

As seen on heatinghelp.com  – March 8, 2017

A High-Rise Residential Facility Case Study

Ventus at Metrogate is a condominium complex located in the greater Toronto area, developed by Tridel Corporation. Upholding the company’s commitment to environmental leadership. Ventus suites boast a number of energy efficient, sustainable features including low voc paints and carpeting, Energy Star® appliances, energy recovery ventilation and high efficiency HVAC systems.

Armstrong originally supplied the pumps that support the HVAC system: two base mounted Series 4030 pumps, configured in parallel mode. Sized to provide 368 gpm at 100 feet of pressure (84 m3/hr at 30 m), each pump was attached to a variable speed drive purchased separately.

Read More

Topics: Uncategorized, HVAC, Prallel Sensorless Technology

Armstrong announces Harley promotion winners

Posted by Armstrong Fluid Technology on Apr 7, 2017, 3:35:06 AM

As seen on mechanical-hub  – March 07, 2017

Toronto —Armstrong Fluid Technology announced that the winners of brand new Harley Davidson Sportster motorcycles in its Cruisin’ with Armstrong promotion were a plumbing contractor and a counter sales person from Texas.

Manuel Lopez, owner of Conquistador Plumbing in Lubbock, Texas, was the winner of the first Harley of a random draw in the Cruisin’ with Armstrong promotion that provided US contractors with a $5 Visa Gift Card and one entry into a draw for the motorcycle every time they purchased an ASTRO or COMPASS circulator.

Read More

Topics: Harley Davidson, In The Media

Armstrong Fluid Technology Employees Donate $10,000 to WaterAid Charity

Posted by Armstrong Fluid Technology on Apr 6, 2017, 9:57:10 AM

As seen on mechanical-hub  – March 14, 2017

Armstrong Fluid Technology announced that its employees have donated $10,000 to WaterAid, an international charity dedicated to providing access to safe water, hygiene and sanitation worldwide.

The Canadian government added another $30,000 in matching funds to bring the total donation to $40,000.

 

Read More

Topics: WaterAid, In The Media

HVAC Pumping Efficiency: Variable Speed Saves Energy in Constant Flow Systems

Posted by Armstrong Fluid Technology on Apr 6, 2017, 9:33:45 AM

As seen on  empoweringpumps – March 07, 2017

Author: Brent Ross, Director, Armstrong Fluid Technology

There is a misconception in the HVAC marketplace that needs to be addressed. Unfortunately, many people believe they only need variable speed when they have variable flow applications. This might be because the recently updated ASHRAE 90.1 2016 rules essentially do not require variable speed in constant flow applications. ASHRAE 90.1 is a minimum requirement, and if there are ways to save more energy than what is required as a “minimum”, we should absolutely be trying to save more energy than what is minimally required. Using variable speed in constant flow systems, the HVAC industry has an opportunity to save an average of 15 to 16% energy and sometimes over 50% and more.

Read More

Topics: Energy Saving, In The Media, Variable speed pumps

The bigger picture

Posted by Armstrong Fluid Technology on Mar 6, 2017, 6:55:23 AM

As seen on  acrjournal – March 03, 2017


Shane Leather, Business Development Manager – Tall Buildings at Armstrong Fluid Technology, looks at energy efficiency strategies for large-scale HVAC installations.

When designing large-scale HVAC installations, the stakes are high. Even seemingly minor design decisions can have major implications when the resulting energy savings (or indeed energy wastage) are scaled up across a large multi-storey building. Achieving outstanding levels of energy efficiency is far from easy in these large-scale projects, however. The challenges fall into a number of categories:

Read More

Topics: Uncategorized, HVAC, In The Media

New Armstrong COMPASS R Represents the Next Technology Evolution for Circulators

Posted by Armstrong Fluid Technology on Mar 6, 2017, 2:06:26 AM

As seen on empoweringpumps.com – April 12, 2017

 

Featuring Advanced Variable Speed Design and New ECM Motors

 

Armstrong Fluid Technology has announced the next technology evolution for circulators with the introduction of the COMPASS R. Featuring advanced variable speed Design Envelope technology, new high-efficiency Armstrong iECMTM motors, and quadratic pressure curves, the COMPASS R will minimize both energy costs and long-term operating costs for homeowners.

Read More

Topics: Compass R, Circulator, In The Media

Hydronics Equipment Growing More Efficient, Intelligent

Posted by Armstrong Fluid Technology on Mar 2, 2017, 5:59:27 AM

As seen on achrnews – February 27, 2017

Many companies showcased their solutions at the 2017 AHR Expo

IMPRESSIVE RESULTS: Armstrong Fluid Technology’s new line of Design Envelope pumps include a new, integrated Armstrong controller that provides a wide range of new functionality, including on-board diagnostics, trending, alerts, and automatic flow-balancing.

LAS VEGAS — Hydronics manufacturers are striving to introduce equipment that is more energy efficient yet encompasses intelligent, simple controls. Many companies showcased their solutions on the 2017 AHR Expo show floor.

Read More

Topics: AHR Expo, Controls, Compass, In The Media

Never miss a thing!

Be the first to get notified

Sign up for our blog notifications and you will be one of the first to know when there is new content. If you want to be in the know, sign up now.

Sign up for notifications now

Recent Posts

Posts by Topic

see all