Armstrong In The Media

4 Reasons to Choose Armstrong Vertical Inline Pumps

Posted by Armstrong Fluid Technology on Aug 21, 2025, 7:28:58 AM

As Seen On: ipsnews.net

 

For decades, centrifugal pumps were typically installed horizontally and bolted to the floor. These base-mounted pumps often proved cumbersome to install and costly to maintain, especially in tight mechanical rooms where space and labor budgets are always under pressure.

Read More

Topics: In The Media, Energy Efficiency, Vertical In-Line, Pump Efficiency, HVAC Pumps, Pump Applications

Armstrong Fluid Technology: Constant Speed Vertical-In-Line Fire Pumps Expansion

Posted by Armstrong Fluid Technology on Mar 10, 2025, 7:49:21 AM
As Seen On: facilitiesnet.com February, 7, 2025
 

The family of Constant Speed Vertical-In-Line Fire Pumps has been expanded with a maximum 500 USGPM flow for both 60hz and 50hz markets and featuring new high-pressure ratings of up to 160PSI. They eliminate the need for offset piping and motor realignment. They also use less floor space than comparable Horizontal Split Case designs.

Read More

Topics: Fire Pumps, HVAC, In The Media, Vertical In-Line

Vertical Turbine Pumps

Posted by Armstrong Fluid Technology on Oct 4, 2024, 9:54:03 AM

 

Profile of Vertical Turbine Pumps

Vertical turbine pumps are specially designed to move water from an underground well or reservoir. Water enters the pump through a bell-shaped part called the suction bell. From there it moves into the first stage impeller, which raises the water's velocity. Vertical turbine pumps are typically used in applications where a flooded suction cannot be maintained. These include applications with underground water sources or below-ground tanks with an above-ground pump room.

Read More

Topics: Fire Pumps, Vertical In-Line

Vertical In-Line Fire Pumps

Posted by Armstrong Fluid Technology on Oct 4, 2024, 9:47:39 AM

 

Vertical in-Line centrifugal pumps are single-stage centrifugal pumps. They are designed for vertical installation with suction and discharge in-line, to provide a smooth flow of liquid through the system. This design aligns the driver, shaft and impeller with gravitational force, so the pumps experience minimal vibration. Vertical In-line pumps serve a wide range of applications, including commercial, municipal and residential high-rise buildings, large industrial premises and storage warehouses, offshore and remote facilities, airports and power stations. Because of their small footprint, they are excellent for industrial applications where space is limited.

Read More

Topics: Fire Pumps, Vertical In-Line

Case study: Heron’s Hill

Posted by Armstrong Fluid Technology on Nov 8, 2023, 11:28:03 AM

Design Envelope 6800 boosters are pre-assembled, compact systems. With Vertical Multi-stage pumps, these systems are energy-efficient and require minimal maintenance for reliable, long-term occupant comfort.

Read More

Topics: Design Envelope, In The Media, 6800 Booster, Vertical In-Line

Case study: Park Hyatt Hotel

Posted by Armstrong Fluid Technology on Aug 17, 2023, 11:36:20 AM


After a major refurbishment to guest suites and event spaces, managers at the Park Hyatt hotel wanted to improve heating efficiency and reduce energy use. Armstrong recommended replacing 1 of 2 existing pumps
with a Design Envelope DEPM pump, to provide a head-to-head efficiency comparison.

Read More

Topics: Case Study, In The Media, Design Envelope pumps, Vertical In-Line

Everything You Need to Know About Armstrong Vertical In-Line Pumps

Posted by Armstrong Fluid Technology on Feb 23, 2023, 8:08:00 AM

As Seen On: factmint.com February 13, 2023

Learn about Armstrong Vertical In-line Pumps and the advantages of this innovative solution for water and wastewater applications. The article will cover the features and benefits of Armstrong Pump Manager and how it can help you save energy. This unique solution includes web-accessible trends, analysis, and automated reports that help you make informed decisions and deliver the highest HVAC performance. You’ll also learn about Armstrong’s Design Envelope, which allows you to save up to 70% on your utility bill.

Read More

Topics: Energy Saving, VIL, In The Media, Pump Manager, Replacement Parts, Vertical In-Line

Never miss a thing!

Be the first to get notified

Sign up for our blog notifications and you will be one of the first to know when there is new content. If you want to be in the know, sign up now.

Sign up for notifications now

Recent Posts

Posts by Topic

see all