Armstrong In The Media

Armstrong Fluid Technology: Constant Speed Vertical-In-Line Fire Pumps Expansion

Posted by Armstrong Fluid Technology on Mar 10, 2025, 7:49:21 AM
email sharing button
As Seen On: facilitiesnet.com February, 7, 2025
FireSet-Vertical-
 

The family of Constant Speed Vertical-In-Line Fire Pumps has been expanded with a maximum 500 USGPM flow for both 60hz and 50hz markets and featuring new high-pressure ratings of up to 160PSI. They eliminate the need for offset piping and motor realignment. They also use less floor space than comparable Horizontal Split Case designs.

Other features of this new model include: 

  • Smaller motor than comparable pumps at the same duty point 
  • Much smaller environmental footprint than standard diesel pumps 
  • UL/ULC and FM approvals 

 

Also Seen On:

 

Topics: Fire Pumps, HVAC, In The Media, Vertical In-Line

Never miss a thing!

Be the first to get notified

Sign up for our blog notifications and you will be one of the first to know when there is new content. If you want to be in the know, sign up now.

Sign up for notifications now

Recent Posts

Posts by Topic

see all