Armstrong In The Media

Armstrong Fluid Technology

Recent Posts

Armstrong Unveils New Customer Loyalty Program for Entire Distribution Channel

Posted by Armstrong Fluid Technology on Jul 10, 2018, 5:36:28 AM

As Seen on empoweringpumps.com – July 03, 2018

Armstrong Fluid Technology has announced the launch of a multifaceted Customer Loyalty Program designed to help North American contractors, wholesalers and sales representatives deepen their customer relationships.

The Contractor Rewards program incentivizes plumbing and HVAC contractors for purchasing Armstrong products by providing them with points that can be redeemed for a variety of prizes ranging from vacations and tools to electronics, recreational equipment and more than 100,000 other valuable items.

Read More

Topics: In The Media, contractor Rewards, Customer Loyalty Program

​​​​​​​Armstrong enhances fire-pump series

Posted by Armstrong Fluid Technology on Jun 27, 2018, 6:10:06 AM

As Seen on worldpumps.com – June 14, 2018

Manufacturer of fluid handling systems, Armstrong Fluid Technology, has announced the addition of two new fire-pump models to its Fireset Horizontal Split Case (HSC) pump line.

The new models, the 5x4x10NF fire pump and the 8x6x15NF pump, were introduced at the US National Fire Protection Association (NFPA) Conference and Expo.

Read More

Topics: HSC Firepak, In The Media, Fireset, NFPA

Armstrong CEO talks sustainability at Global Energy Summit

Posted by Armstrong Fluid Technology on Jun 27, 2018, 3:31:23 AM

As Seen on pmmag.com – June 20, 2018

 

Lex van der Weerd, CEO of Armstrong Fluid Technology, discusses the company’s long-term plans to reduce GHG (greenhouse gas) emissions through new technologies, programs and educational efforts around the globe during the company’s Global Energy Summit June 20 in Toronto.

Read More

Topics: Sustainability, In The Media, Global Energy Summit

Armstrong partners with industry leaders on “2 by 22” GHG Initiative

Posted by Armstrong Fluid Technology on Jun 27, 2018, 3:21:22 AM

As Seen on pmengineer.com – June 19, 2018

 

Armstrong Fluid Technology has announced an initiative to reduce Greenhouse Gas (GHG) emissions by 2 million tons by the year 2022 and issued a challenge to industry participants to set similarly aggressive targets for the same 4-year time frame.

“Organizations globally are being driven to achieve a zero footprint future. We believe this can best be achieved through key stakeholders focusing on solutions and timelines that will make zero footprint a near-term reality,” said Lex van der Weerd, Armstrong’s CEO. “We are both inviting and challenging all organizations to join us in pursuing the goal of zero footprint operations.”

Read More

Topics: Sustainability, In The Media, Greenhouse Gas (GHG), Global Energy Summit

Fire-protection manufacturers emphasize innovation

Posted by Armstrong Fluid Technology on May 31, 2018, 10:16:17 AM

As Seen on pmengineer.com – May 23, 2018

With the 2018 NFPA Expo right around the corner — set for June 11-14 at the Mandalay Bay Convention Center in Las Vegas, Nevada — fire-protection product manufacturers are thinking next-level.

“We definitely have tried to get back to that innovation mindset,” Lubrizol National Strategic Accounts Manager Anthony Spencer says. “For awhile we stagnated and allowed CPVC pipe to just stay where it was.”

Read More

Topics: In The Media, Fire-protection, NFPA, NFPA 2018 Expo

Energy-efficient fire pumps from Armstrong Fluid Technology

Posted by Armstrong Fluid Technology on May 31, 2018, 10:10:46 AM

As Seen on pmengineer.com – May 22, 2018

Armstrong Fluid Technology updates its Fireset Horizontal Split Case Pump line with two new models: a 5x4x10NF fire pump for installs requiring 500 gpm at pressures from 55 to 167 psi and a 8x6x15 option for applications requiring flows between 1,500 and 2,000 gpm at pressures from 54 to 168 psi. The new Fireset HSC pumps have double suction design for operating efficiency and high-flow performance, right- or left-hand suction configuration with electric-driven pumps for adapting to mechanical room piping arrangements and a compact design for easy installation and maintenance.

Read More

Topics: Fire Pumps, In The Media, Fireset, HSC

Armstrong Introduces the Stainless Steel COMPASS R High-Efficiency Circulator

Posted by Armstrong Fluid Technology on May 31, 2018, 9:40:48 AM

As Seen on empoweringpumps.com – May 22, 2018

Armstrong Fluid Technology has announced that its next technology evolution COMPASS R20-75 circulator is available in a stainless steel construction.

Designed for use in potable water systems, the new stainless steel model features a dry rotor design, as well as advanced variable speed Design Envelope technology, Armstrong iECMTM motors, and quadratic control to minimize both energy costs and long-term operating costs for homeowners.

Read More

Topics: Compass R, In The Media, Stainless Steel, Compass R SS

Armstrong Unveils New Integrated Tower Control System (ITC 9521)

Posted by Armstrong Fluid Technology on Apr 13, 2018, 5:22:09 AM

As Seen on empoweringpumps.com – April 11, 2018

Armstrong Fluid Technology announces the introduction of the new ITC 9521, an Integrated Tower Control System designed to transform an HVAC installation into an intelligent system for a variety of heat rejection applications.

“Leveraging Armstrong’s advanced demand-based algorithms and industry-leading Parallel Sensorless technology, the ITC 9521 provides users with an energy-efficient solution for heat rejection processes for applications such as datacenters, condensing cooling, heat pumps, paint processing, injection molding and air-compressor stations,” according to Lex van der Weerd, Armstrong CEO.

Read More

Topics: Controls, In The Media, ITC 9521, Integrated Tower Control System

Armstrong launches high performance fire pump models

Posted by Armstrong Fluid Technology on Feb 6, 2018, 9:09:08 AM

As Seen on arabianindustry.com – January 23, 2018

Armstrong Firesetpumps feature a double suction design for superior levels of operating performance.

Armstrong Fluid Technology will be debuting a new line of high performance fire pump models at Intersec 2018 in Dubai. 

The Armstrong Fireset Horizontal Split Case (HSC) fire pumps offer superior flow performance and incorporate features for ease of installation and maintenance.

Read More

Topics: Fire Pumps, In The Media

Armstrong Announces TowerMax Optimization Service

Posted by Armstrong Fluid Technology on Feb 6, 2018, 7:18:16 AM

Armstrong Fluid Technology has announced a new service that will provide up to 25% savings compared to traditional variable speed plant operation.

TowerMax is an optimization service that boosts energy and water savings, and is available as an upgrade for any previous installation of an Armstrong Design Envelope IPC 9521 plant controller. TowerMax employs advanced operating algorithms to minimize the energy and water consumption of a variable speed chiller plant.

Read More

Topics: In The Media, TowerMax, Optimization Service

Never miss a thing!

Be the first to get notified

Sign up for our blog notifications and you will be one of the first to know when there is new content. If you want to be in the know, sign up now.

Sign up for notifications now

Recent Posts

Posts by Topic

see all