Armstrong In The Media

Armstrong Fluid Technology

Recent Posts

Pumping up Glasgow Regeneration

Posted by Armstrong Fluid Technology on Feb 3, 2016, 4:37:46 AM

As seen on This Weekin FM.com - January 22, 2016

 
By Mike Gannon
 
An fully integrated packaged plant room for the HVAC of a new development in Glasgow has speeded the installation and reduced traffic at the busy city centre site.

The supplier – Armstrong Fluid Technology – played a key role in the delivery of the Connections project at 110 Queen Street, Glasgow with a fully integrated packaged plant room handling the HVAC system in the building.

Read More

Topics: Armstrong Fluid Technology, HVAC, In The Media

Revved Up at the Harley Factory

Posted by Armstrong Fluid Technology on Feb 3, 2016, 3:58:24 AM

As seen on The NEWS - January 25, 2016

 

LET'S ROLL: A selection of Harley-Davidson motorcycles was on display at the historic Harley-Davidson factory where Armstrong Fluid Technology hosted its expo party.
Read More

Topics: AHR Expo, Events, In The Media

Armstrong Introduces New Energy-Savings Horizontal End Suction Pumps Featuring Integrated Controls

Posted by Armstrong Fluid Technology on Feb 3, 2016, 2:54:08 AM

As seen on HeatingHelp.com - February 1, 2016

Armstrong Fluid Technology announces the introduction of two new series of Horizontal End Suction Design Envelope (DE) Pumps featuring Sensorless integrated controls for greater energy savings.

Both the DE 4200H and DE 4280 Series include Armstrong Design Envelope technology, with easy-to-use Sensorless control and enhanced connectivity to BAS to achieve significant efficiency improvements. The DE 4200H pumps are supplied with split-couplings and outside balanced seals while the DE 4280 pumps use a close-coupled design.

Read More

Topics: Design Envelope, Horizontal Endsuction, In The Media

Armstrong unveils improved Astro 2 hot water recirculation systems

Posted by Armstrong Fluid Technology on Feb 3, 2016, 2:47:16 AM

As Seen on Healthcare Facilities Today - February 2, 2016

Armstrong Fluid Technology has introduced new versions of the popular Astro 2 Hot Water Recirculation (HWR) pumps.  A hot water recirculation system can save a typical family over 12,000 gallons of water per year by eliminating the waste of water that occurs when occupants open a hot water faucet and have to wait for hot water to reach the fixture.

Astro 2 HWR circulators are suitable for use in a 3-pipe installation with a dedicated return. The Astro Express 2 System includes the innovative Astro Express LF Valve and is designed for use in a standard residential 2-pipe installation.

Read More

Topics: Astro2, Circulator, In The Media

Optimising Energy Efficiency of Cooling Systems: A Guide for Facilities Managers

Posted by Armstrong Fluid Technology on Feb 1, 2016, 2:26:52 AM

As seen on Facilities the Industry Yearbook 2016 

By Steve Cooper, Director – Sustainable Design, Armstrong Fluid Technology

Facilities managers with responsibility for air conditioned buildings often ask how they can improve energy efficiency and drive down utility bills. Typically, access to information is not the problem. The latest BMS technology provides sophisticated data collection and display, with the ability to manipulate data to create statistical reports. The difficulty is how to take the next step - tackling the environmental performance of the building with practical measures (that do not require complete replacement of existing HVAC plant).

Read More

Topics: Armstrong Fluid Technology, Magazine, In The Media

2016 AHR Expo

Posted by Armstrong Fluid Technology on Jan 28, 2016, 1:41:10 AM

As seen on reevesjournal.com – January 2016

AHR Product Preview

The steak is just meat without some sizzle to go with it

 

Trade shows feature show floors for a reason.

 

Contractors will generally find that trade shows have a lot to offer. Between all the networking and social events, entire days of show attendance can be taken up by educational pursuits and seminars alone. Throw in a round of golf if there’s time and there you have your basic meat-and-potatoes trade show event.

Read More

Topics: AHR Expro, Design Envelope, In The Media

Rocking with Santa

Posted by Armstrong Fluid Technology on Jan 5, 2016, 7:07:06 AM

As seen on kentonbee.our-hometown.com – December 23, 2015

Rocking with Santa sees another successful year

Rocking with Santa, an event to close the 15th annual toy drive in Ken-Ton, served the largest number of families in its history.

More than 150 families were able to go home with three gifts per child in addition to stocking stuffers for all, according to John White, who has run the event since it began.

Read More

Topics: In The Media

USGBC's message is received at 2015 Greenbuild Expo

Posted by Armstrong Fluid Technology on Dec 21, 2015, 4:54:59 AM

The sustainable plumbing, HVAC and construction industry made its message known in the nation’s capital.

As seen on pmengineer.com – December 17, 2015

 

2015 Greenbuild Expo
Steven Lane, Armstrong Fluid Technology’s vice president of communications, speaks at an after-hours event during the 2015 Greenbuild Expo at the Washington Convention Center in Washington, D.C.Photo by John McNally/pme

 

The sustainable plumbing, HVAC and construction industry made its message known in the nation’s capital Nov. 17-20 at the 2015 Greenbuild Expo at the Washington Convention Center in Washington D.C.

Read More

Topics: Armstrong Fluid Technology, Energy - saving pumps, GreenBuild, In The Media

Want to Curb Your HVAC System’s Energy Thirst?

Posted by Armstrong Fluid Technology on Dec 10, 2015, 7:50:16 AM

As seen on cabuildingsnews.com – December 2015

Manufacturers and Service Providers Offer a Variety of Products and Strategies

HVAC SYSTEMS CAN USE AS MUCH AS 40% OF A BUILDING’S ENERGY, says the utility company Pacific Gas & Electric. “When properly designed, implemented, and operated, these systems ensure the comfort of the people in the facility in addition to ensuring the quality and financial viability of the processes and products produced. However, while simple in concept, most air handling systems are dynamically com­plex and highly interactive. A disturbance in one element can ripple out and affect the stability and viability of the entire system and the utility systems serving the air handling unit. In some cases, these issues manifest themselves in a manner that demands correction; tenants complain, product quality becomes substandard, or in extreme cases, the area serves becomes un-inhabitable.

Read More

Topics: HVAC, In The Media

Motor Technology Drives Circulator Pump Innovation

Posted by Armstrong Fluid Technology on Dec 8, 2015, 6:41:42 AM

As seen on achrnews.com – December 7, 2015

Variable-speed technology and controls improve pump efficiency, ease of installation

In hydronic heating and cooling systems, circulator pumps move water or refrigerant throughout a closed-loop system in order to transfer energy from the source to the point of need. While older circulator pumps utilized single-speed motors and were largely inefficient, advances in motor technology, controls, and pump design have transformed the market and ushered in a new era of highly efficient products that feature variable-speed motors, easy installation and setup, remote connectivity, and more.

Read More

Topics: Circulator, In The Media

Never miss a thing!

Be the first to get notified

Sign up for our blog notifications and you will be one of the first to know when there is new content. If you want to be in the know, sign up now.

Sign up for notifications now

Recent Posts

Posts by Topic

see all