Armstrong In The Media

Armstrong Fluid Technology

Recent Posts

CEO first at Armstrong

Posted by Armstrong Fluid Technology on May 20, 2011, 8:26:59 AM

As seen on worldpumps.com - May 20, 2011

Canadian pump manufacturer SA Armstrong Ltd has appointed its first CEO in the company’s 77-year history.

In this new role at Armstrong, Alexander G van der Weerd will be responsible for the formulation and execution of the company’s global business strategy.

Read More

Topics: Uncategorized

Pump systems improve energy efficiency

Posted by Armstrong Fluid Technology on Mar 15, 2011, 6:27:39 AM

As seen on worldpumps.com - March 15, 2011

Armstrong has launched a series of pre-designed packaged pump solutions that have improved energy efficiency and reduced footprint.

Read More

Topics: Armstrong Fluid Technology, worldpumps.com

Armstrong offers smaller expansion system

Posted by Armstrong Fluid Technology on Jan 8, 2011, 11:09:22 PM

As seen on worldpumps.com - January 9, 2011

Armstrong has launched Armex II, a new range of high volume pressurisation and degassing systems in its Armex range.

Armex II manages the expansion and contraction of heating and cooling system water, and providing automatic water make-up. It also offers dissolved gas deaeration within the same self-contained system.

Read More

Topics: Armstrong Fluid Technology, worldpumps.com, In The Media

Armstrong International wins Industry Innovation Award

Posted by Armstrong Fluid Technology on Nov 18, 2010, 12:18:30 AM

As seen on worldpumps.com - November 18, 2010

Armstrong’s Brain Model DRV80 has thousands of successful installations and is the basis for design at some of the world’s largest and most prestigious hotel chains, retirement communities and consulting plumbing engineering firms. Armstrong introduced the first electronic Brain in 2005 and has since expanded its digital technology platform. Most recently, Armstrong displayed an ASSE 1070 compliant digital hands free six-outlet valve for lavatories and a 1016 compliant version for showers. Certification testing is in process.

Read More

Topics: Armstrong Fluid Technology, worldpumps.com

Armstrong offers online energy saving guide

Posted by Armstrong Fluid Technology on Nov 16, 2010, 2:37:56 AM

As seen on worldpumps.com - November 16, 2010

The free, 8 page energy saving guide identifies various upgrade options and their paybacks, including detailed scenarios suggesting the types of systems which might be suitable.

Read More

Topics: Armstrong Fluid Technology, Energy Efficient, worldpumps.com, In The Media

Armstrong adds new manufacturing plant in China

Posted by Armstrong Fluid Technology on Nov 11, 2010, 7:21:26 AM

As seen on worldpumps.com - November 11, 2010

Armstrong has officially opened a new manufacturing facility in China.

The 30 000 sq ft Armstrong Fluid Systems Shanghai facility is the company’s third manufacturing plant in Asia, and ninth globally.

Located just outside Shanghai, the new facility houses manufacturing, assembly and testing for commercial pumps, circuit balancing valves and Flo-Trex valves, along with all aspects of finance, procurement, logistics, field service and commissioning of integrated plant controls.
Read More

Topics: Armstrong Fluid Technology, worldpumps.com

Armstrong extends variable speed booster set range

Posted by Armstrong Fluid Technology on Oct 5, 2010, 8:31:20 AM

As seen on worldpumps.com - October 5, 2010

The new models in the 6800 IVS range incorporate the Soft Fill feature which reduces the risk of hydraulic shock damage and water hammer.

Armstrong's 6900 IVS range has been extended to offer booster sets up to 25 bar, and variable speed above 7.5 kW. The motor size limit is 45 kW, but there is a choice of 2, 3, 4, or 5 pumps for each set to suit the widest range of applications. The 6800 IVS series of booster sets is designed for buildings such as schools, hotels and hospitals, and design features such as Soft Fill enable the range to be used in high-rise residential and commercial buildings.

Read More

Topics: Armstrong Fluid Technology, worldpumps.com

Armstrong to launch carbon solutions under ECO:nomics brand

Posted by Armstrong Fluid Technology on Jul 20, 2010, 12:03:03 AM

As seen on worldpumps.com - July 20, 2010

Each solution is designed to offer a lower carbon footprint, enabling customers to meet sustainability goals without elevating capital costs.

Read More

Topics: Armstrong Fluid Technology, worldpumps.com

Armstrong integrates UK operations

Posted by Armstrong Fluid Technology on Jun 17, 2010, 12:24:21 AM

As seen on worldpumps.com - June 17, 2010

Armstrong’s off-site construction division, Armstrong Integrated Systems based in Halesowen, and the HVAC equipment business headquartered in Manchester and Redhill will now operate as a single company, Armstrong Integrated Ltd, under a new legal framework.

Armstrong says the changes are designed to support the company’s continued growth in the UK market and do not involve any scaling down of activities. Operations will continue at all three sites – Halesowen, Manchester and Redhill – with the existing workforce and management structure.
Read More

Topics: Armstrong Fluid Technology, worldpumps.com

Armstrong 55 kW drives for control range

Posted by Armstrong Fluid Technology on Apr 30, 2010, 5:01:29 AM

As seen on worldpumps.com - April 30, 2010

Armstrong has extended its IVS range of sensorless control pumps to include models with variable speed drives up to 55 kW. Previously, the drives were only available up to 7.5 kW.

Armstrong is also launching a range of standalone inverters, the IVS102, to offer specifiers variable speed pumping up to 450 kW maximum power. These inverters which automatically calculate the building demand and adjust the speed of the drives accordingly.

Read More

Topics: Armstrong Fluid Technology, Design Envelope, worldpumps.com

Never miss a thing!

Be the first to get notified

Sign up for our blog notifications and you will be one of the first to know when there is new content. If you want to be in the know, sign up now.

Sign up for notifications now

Recent Posts

Posts by Topic

see all