As seen on healthcarefacilitiestoday.com - August 29, 2014
TORONTO - Armstrong Fluid Technology has announced the expansion of its Astro wet-rotor circulator offering with the introduction of the Astro 2 Series. Featuring four new sizes, the Astro 2 Series now offers flange-to-flange and bolt-to-bolt compatibility with 100% of competing models in terms of performance.
Designed for fast and convenient installation and years of trouble-free operation, the new models also address a broader range of applications. Key features include: three field-selectable operating speeds, double the head and triple the flow, a plug-in terminal strip to save time on installation, e-coating on the inside of the cast iron volutes to provide enhanced corrosion protection, pre-installed high-flow check valve and availability in cast iron, stainless steel and lead-free bronze.
In addition, Armstrong has announced an industry-leading five-year warranty on both the Astro and Compass Circulators. Commenting on the company’s commitment to a five-year warranty, Rod Hightower, Armstrong’s Commercial Director, US stated, "The five-year warranty is a reflection of the quality and reliability built into these products."
Also seen on:
- cemag.us - August 26, 2014
- facilitiesnet.com - August 26, 2014
- worldpumps.com - August 27, 2014
- waterwastewaterasia.com - August 27, 2014
- impeller.net - August 28, 2014
- pump-world.com - August 28, 2014
- pumps-processes.com - August 28, 2014
- pumpselection.net - August 28, 2014
- heatinghelp.com - August 2014
- digital.bnpmedia.com - August 2014
- esmagazine.com - September 1, 2014
- csemag.com - September 4, 2014
- labdesignnews.com - October 8, 2014
- psmena.imirus.com - November 2014
- plumbermag.com - February 18, 2015