Armstrong In The Media

Armstrong Fluid Technology

Recent Posts

Using the Gift of Talent to Give the Gift of Water

Posted by Armstrong Fluid Technology on Sep 1, 2016, 2:39:06 AM

As Seen on empoweringpumps.com – August 30, 2016

 

I can’t juggle. I can’t act. I can’t sing. But if I could upload a video of myself doing all three things just to raise money to help people gain access to clean water, I’d do all three in a heartbeat. Currently, this is an opportunity open to the employees at Armstrong Fluid Technology.

Read More

Topics: Armstrong Fluid Technology, Awards, In The Media

2016 Frost & Sullivan - Best practices award

Posted by Armstrong Fluid Technology on Aug 18, 2016, 7:22:14 AM

Armstrong Fluid Technologies Award Write Up - Download

The global consulting firm Frost & Sullivan has recognized Armstrong Fluid Technology for excellence in Product Line Strategy, selecting Armstrong to receive the 2016 Best Practices Award.

 

“We are very honored to win this prestigious Best Practices Award and to have our Design Envelope technology recognized for its exceptional Product Line Leadership”
Lex van der Weerd, Armstrong CEO.

 

Frost & Sullivan, the Growth Partnership Company, works in collaboration with clients to leverage visionary innovation. For more than 50 years, they have been developing growth strategies for companies around the world.

Read More

Topics: Armstrong Fluid Technology, In The Media

Energy savings at office complex

Posted by Armstrong Fluid Technology on Aug 17, 2016, 8:57:51 AM

As Seen on WorldPumps – September, 2016

When a major commercial building in the centre of Birmingham needed to refurbish the site’s HVAC pumping system, Armstrong Fluid Technology came up with an alternative solution which reduced energy consumption and improved efficiency.

The Axis office complex occupies a 178,000 sq. ft site close to Broad Street and Birmingham New Street Station. The 11-storey building has recently undergone a major HVAC refurbishment and Armstrong Fluid Technology was asked to provide a proposal for the project. The existing pumps, which were fixed speed end suction models, were reaching the end of their useful life.

Read More

Topics: Armstrong Fluid Technology, Energy Efficient, HVAC, In The Media

Armstrong Fluid Technology Hosts Energy Summit in Canada

Posted by Armstrong Fluid Technology on Aug 17, 2016, 8:07:17 AM

As Seen on plumbingengineer.com – August, 2016

Since 2008, Armstrong Fluid Technology has been spreading the word about how its Design Envelope technology when applied to HVAC and fluid flow systems achieves high efficiency, and low installed cost, operating cost, environmental cost, and project operating risk. As a result, energy has become an integral part of Armstrong’s conversations. So, it was fitting that from June 27-29, the company gathered nearly 300 attendees from around the world for its biennial summit themed, “Making Energy Make Sense.”

Read More

Topics: Armstrong Fluid Technology, In The Media, Summit

Armstrong Fluid Technology Announces New Variable Speed Retrofit Package

Posted by Armstrong Fluid Technology on Jul 19, 2016, 12:46:54 AM

As Seen on heatinghelp.com - July 18, 2016

The Design Envelope Vertical-In-Line Retrofit allows building owners to replace the moving parts of an installed Armstrong constant speed pump while retaining the existing pump casing, insulation and piping. This new solution reduces the costs for equipment, shipping and scrap as well as installation labor.

The Design Envelope Vertical-In-Line Retrofit provides owners of existing constant speed pumps with an opportunity to save up to 70% on energy costs by upgrading to variable speed. Design Envelope technology accommodates future changes in flow requirements and its variable speed operation means longer equipment life (20%-30%), and greater reliability.

Read More

Topics: Design Envelope, Retrofit, VIL, HVAC, In The Media

An Interview With Robert Dietrich of Armstrong Fluid Technology

Posted by Armstrong Fluid Technology on Jul 19, 2016, 12:16:18 AM

Canadian-headquartered Armstrong Fluid Technology has been a Hodgson Russ client for more than 50 years. CFO Robert Dietrich discusses the benefits the company has experienced from this long ­term relationship.

Read More

Topics: In The Media

Renewable onsite power generation from packaged biomass systems

Posted by Armstrong Fluid Technology on Jul 13, 2016, 3:24:30 AM

As seen on efficientenergy.net – July 08, 2016

Packaged biomass boiler systems from Armstrong Fluid Technology have been instrumental in delivering one of the UK’s largest ever distributed heat project. A total of 72 bespoke biomass boiler systems were off-site manufactured by the company for installation in Bernard Matthews farm sites across the east of England, making it possible to deliver this massive biomass project effectively within the necessary timescales.

Read More

Topics: Boilers, In The Media, packaged plant

Keep Your Eye on These 3 HVAC Updates (#1. Pump Efficiency)

Posted by Armstrong Fluid Technology on Jul 12, 2016, 5:50:15 AM

As seen on facilitiesnet.com – July 2016

Part 1 of a 3-part article on why VRFs are gaining ground, popular refrigerants may be phased out, and pumps present an overlooked way to save energy.

By Rita Tatum July 2016

Once it has been designed and installed, the HVAC system is something the facility manager has to live with for a long time. Heating and cooling equipment has a long life cycle, and because of the cost of replacement, it may well be kept in service even after the end of its projected useful life.

Read More

Topics: Armstrong Fluid Technology, HVAC, In The Media

Armstrong Fluid Technology Stainless Steel Compass Circulator Energy Saving DE Model

Posted by Armstrong Fluid Technology on Jul 11, 2016, 2:43:17 AM

As seen on thewholesaler.com – July 2016

 

Armstrong Fluid Technology’s new stainless steel COMPASS wet rotor circulator featuring its innovative Design Envelope (DE) energy saving technology. COMPASS circulators offer high flow capacity and eight optional control modes that deliver superior energy efficiency for lower operating costs. The new SSU Model also features a threaded union connection that is easy to adapt to copper, PEX or CPVC plumbing.

Read More

Topics: Design Envelope, Circulator, Compass, In The Media

Armstrong Fluid Technology Announces New Size of HSC Firepak™ for 300 psi

Posted by Armstrong Fluid Technology on Jun 21, 2016, 3:37:39 AM

As seen on HeatingHelp.com – June 13, 2016

TORONTO — Armstrong Fluid Technology has introduced its enhanced HSC Firepak™, a completely integrated fire pump solution that delivers a unique set of advantages to both designers and contractors.

Featuring a compact design for fast and easy installation, Armstrong’s “Plug and Leave” design provides fire safety professionals with a complete fire pump solution that offers:

Read More

Topics: Fire Pumps, HSC Firepak, In The Media

Never miss a thing!

Be the first to get notified

Sign up for our blog notifications and you will be one of the first to know when there is new content. If you want to be in the know, sign up now.

Sign up for notifications now

Recent Posts

Posts by Topic

see all