As Seen On: fluidhandlingmag.com October 28, 2020
Armstrong Fluid Technology has announced that its Design Envelope pumps are available with a three-day quick-ship delivery time.
Encompassing the most widely-used Armstrong pumps for commercial-scale applications, the delivery includes Vertical In-Line, End Suction and Tango models.Kevin Goodison, wholesale distribution sales manager for Armstrong Fluid Technology said: “Our three-day delivery time will help customers by shortening project schedules and reducing downtime, especially in breakdown situations. We’re delighted to be the first in our sector to offer quick-ship delivery times on these larger, commercial scale pumps.”
Until December 31st, Armstrong Fluid Technology is also offering customers a three-month free trial of Pump Manager.
Pump Manager leverages the embedded intelligence and connectivity available through Armstrong Design Envelope pumps to support Active Performance Management of building performance.
Customers will have free access to the Pump Manager essential features, including real-time insight and alerts for up to 4 pumps.
For more information contact 08444 145 145, email sales@armstrongfluidtechnology, or visit armstrongfluidtechnology.com
Also Seen On
- estaenergy.org.uk - October 22, 2020
- worldpumps.com - October 26, 2020