Armstrong In The Media

Armstrong Fluid Technology: Three keys to lower HVAC costs

Posted by Armstrong Fluid Technology on Nov 23, 2021, 11:56:59 PM

As Seen On: manufacturingtodayindia.com November 12, 2021

Most pump control systems support variable-speed operation, but they don’t provide web-based alerts or notifications of changes to settings.

 Pump Manager

Armstrong Fluid Technology, HVAC, Permanent Magnet motor technology, pump Manager, Sensorless Pump Control (PSPC)

Motor Efficiency - Permanent Magnet motor technology reduces efficiency losses, for improved performance and efficiency. Why is this important? Compared to standard induction motors, the latest Permanent Magnet motors deliver an efficiency improvement of 3-12% at full load and even more under part load. The difference in lifetime energy costs could be over a thousand dollars! Just from the motor choice on one pump!!

Remote Performance Tracking with Alerts - Most pump control systems support variable-speed operation, but they don’t provide web-based alerts or notifications of changes to settings. Why is this important? In buildings around the world, untold numbers of variable speed pumps have been set to ‘In-hand’ mode and accidentally left operating at constant speed – a huge waste of energy. The latest cloud-based services for performance tracking can send alerts for common issues including changes to settings, such as a pump set to ‘In-hand’ mode.  Pump Manager helps to ensure you get the full benefit of the pump operating at the best possible efficiency levels. If there’s a problem, you’ll hear about it.

Parallel Pumping - Even if there’s no need for redundancy, parallel pumping using Parallel Sensor less Pump Control (PSPC) is the way to go. On top of the energy savings from variable speed, you’ll save an extra 30% on your pump energy costs by using efficiency-based staging.

Also Seen On 

 

Topics: HVAC System, Pump Manager, Performance Management, Parallel Pumping Systems, Energy Efficiency, Permanent Magnet Motors

Never miss a thing!

Be the first to get notified

Sign up for our blog notifications and you will be one of the first to know when there is new content. If you want to be in the know, sign up now.

Sign up for notifications now

Recent Posts

Posts by Topic

see all