Armstrong In The Media

Can We Do Better? Understanding the U.S. Department of Energy / NRCAN 2020 Pump Regulations

Posted by Armstrong Fluid Technology on Feb 25, 2020 10:01:59 AM

As Seen On: empoweringpumps.com February 01, 2020

DE_Installationnew

As of January 27th, 2020, newly manufactured pumps are required to meet the new U.S. DOE/NRCAN 2020 Pump Efficiency Regulations standards. The primary objective of the new regulations is to reduce energy consumption. Secondary items include cost savings for businesses using regulated energy products, and reduction of unnecessary regulation differences between the EU, Canada, and the United States. While the new U.S. DOE 2020 rules establish minimum energy efficiency requirements, the reality is these requirements represent the least we can do

Efficiency standards that are more stringent are certainly a welcome change. However, it should be pointed out that there are issues with the methods used to calculate efficiencies (see side bar on page 2). A recent on-demand webinar provides some background on the issue (watch this 29-minute video at your convenience). While the use of the U.S. DOE / NRcan Pump Energy Index (PEI) ratings is valuable to determine a minimum energy standard, the pump with the lowest PEI may not provide the best energy efficiency in an operating environment.  

Scope of US DOE / NRcan 2020
Regulations:

Clean Water Pump is one of the following types:

  • an end suction close-coupled pump with a specific speed not more than 5000
  • an end suction frame mounted-pump with its own bearings and with a specific speed not more than 5000
  • an in-line pump
  • A radially split, multi-stage, vertical, in-line diffuser casing pump, or
  • a submersible turbine pump with a bowl diameter not greater than 152 mm (6 in)

Specifications for pumps included in the regulations:

  • Shaft input power between 1 – 200 HP inclusive at (BEP)
  • Flow rate > or = 25 gpm (BEP) with a full impeller diameter
  • Maximum Head < 459 ft at (BEP)
  • Design temperature range between 14 to 248 degrees Fahrenheit
  • Designed to operate with either 2 poles or 4 poles induction motor or non
    induction motor with nominal speed 3600 RPM (2880 – 4320) and 1800 RPM
    (1440 – 2160)

DOES NOT include the following:

  • fire pump
  • self priming pump
  • prime-assist pump
  • magnet-driven pump (not to be confused with Design Envelope Permanent Magnet Motors)
  • pumps designed for nuclear facilities or to military specs
  • pool pumps and circulators (*covered under a separate regulation)

 

The issue is that the calculation method does not consider overall efficiency. It focuses instead on efficiency at a particular operating point of the load profile. But that approach doesn’t make the best sense, because HVAC is a part-load application.  And although that fact may not be in dispute, it’s not as well understood just how much of the time in any given season requires part-load operation. HVAC systems run at their full output for approximately 3% of operating hours (on average). For the other 97% of a given season the equipment operates below capacity along a range of duty points. What matters for HVAC efficiency, energy savings and GHG reductions is the pump efficiency across the entire range of performance points.  In practice, pumps that offer intelligent variable speed control are more than twice as efficient. A Design Envelope pump with a PEI of 0.4 would consume only 40% of the energy a minimally compliant pump would require. And an intelligent connected pump would maintain that high efficiency performance longer.

Naturally then it’s important to select a pump according to the best efficiency across the appropriate range of output. Most design engineers use pump selection software. As part of that selection process they must make sure they’re using software that selects a pump on the basis of a range of performance rather than a single duty point. 

Pump Energy Index Definitions:

PEI – Pump Energy Index

  • As of January 27, 2020, any pump manufactured should have a PEI < OR = 1 and nameplate labeled with Model Number, PEI, Impeller size to be sold in Canada &amp; USA.
  • PEI CL – Pump Energy Index for Bare pump and Pump + Motor
  • PEI VL – Pump Energy Index for Pump + Motor + VFD Controls PER – Pump Efficiency Rating
  • PER CL – Pump Efficiency Rating for Bare pump and Pump + Motor
  • Per VL – Pump Efficiency Rating for Pump + Motor + VFD Controls

Pump Energy Index Key Points:

The PEI is the PER divided by a calculated minimally compliant PER for the given pump model.

The lower the Pump Energy Index, the more efficient the pump is:

PEIcl average range is from 0.75 – 1.0 and

PEIvl average range is from 0.4 – 0.55.

PEIvl is significantly better than PEIcl.

 

Unaddressed Energy Opportunities for Energy Savings 

Including pump efficiency in the consideration criteria for a pump is great and using the right approach to find the most efficient pump for the whole range of operating points is even better. But the DOE regulations miss an important opportunity for energy savings.  Focusing on new pump installations they will ensure new pumps are more efficient than they might otherwise be, but what about installed equipment in existing buildings? Due in part to established sizing habits, the pumps in most HVAC systems all over North America are over-sized and the energy waste caused by inefficiency is absolutely staggering. In the US alone an astronomical amount of energy is lost every year in HVAC systems caused by performance drift – the gradual degradation of efficiency due to changes in settings or aging of equipment. With so much potential for savings, building owners and operators would be well served to look carefully at their HVAC systems and components and consider retrofits – whether or not they are legally mandated to do so. 

 

Armstrong pump retrofit building hvac upgrade

Consider a retrofit project to be a sequential process of finding and leveraging performance date. Don’t start by replacing the biggest energy draw. Start with the component that can tell you the most – your pump.

Most people who take the initiative to start the retrofit process begin by looking at the chiller, assuming this is the biggest ‘energy hog’. Replacing the chiller often produces a change in energy consumption, but delivers no more insight into the performance of the overall system. If instead a project is started with a retrofit to a smart pump, users can obtain detailed information about flow rates and system conditions.

 

 

Flow Informs.

The most reliable and informative connecting element in your HVAC system is the fluid flow. Flow rates inform decisions on operating speeds and equipment choices. With flow data to work with, you become empowered to retrofit other system components based on a far more detailed understanding of how the HVAC system operates.  

Bring an informed, system-wide perspective to HVAC performance and efficiency. When you take a step-by-step approach to achieving better energy efficiencies based on deepening performance insights, efficiency can improve at every step. At each stage of the project, you’ll have more information to work with and more savings from the earlier stages to help pay for the next component upgrades, so you can upgrade your systems in a manner that is much more financially responsible. Plus, you get to an end result that is so much more impactful than if you just took the approach of retrofitting the ‘biggest piece of equipment in the room’.

APMText

 

Learn more about Energy Upgrades at bit.ly/ArmstrongEnergyUpgrade.

 

Topics: Energy Saving, In The Media, Energy Efficiency, Standards & Regulations

Never miss a thing!

Be the first to get notified

Sign up for our blog notifications and you will be one of the first to know when there is new content. If you want to be in the know, sign up now.

Sign up for notifications now

Recent Posts

Posts by Topic

see all