Armstrong In The Media

Parallel Sensorless Pump Control best-efficiency staging

Posted by Armstrong Fluid Technology on Jul 18, 2022 3:44:34 AM

As Seen On: constructionweekonline.in July 6,2022

It’s important for HVAC system designers to understand that the relationship between pump costs and pump size is not a simple straight line. As pump sizes increase, the costs for the equipment, related components and installation increase faster. The result is that a pumping system that serves an HVAC load using two small pumps is less expensive than buying and installing one large pump.

Read More

Topics: Best efficiency staging, HVAC System, In The Media, Parallel Sensorless Pump Controller, Parallel Pumping Systems

British Pump Manufacturers Association honors Armstrong Fluid Technology

Posted by Armstrong Fluid Technology on May 3, 2019 10:52:38 AM

As Seen on esmagazine.com - April 29, 2019

Armstrong Fluid Technology's Design Envelope Tango pump has been awarded the Environmental Contribution of the Year at the 2019 BPMA Pump Industry Awards.

Founded by the British Pump Manufacturers Association (BPMA) in 2000, the Pump Industry Awards program celebrates the achievements of pump companies and individuals

Read More

Topics: Awards, In The Media, Parallel Sensorless Pump Controller, Tango, BPMA

Armstrong Parallel Sensorless Pump Controller Wins CIPHEX WEST'S Most-Innovative Product Award

Posted by Armstrong Fluid Technology on Jan 5, 2015 7:05:53 PM

As seen on heatinghelp.com - December 15, 2014

Armstrong Fluid Technology’s Design Envelope Parallel Sensorless Pump Controller (PSPC) has been selected as the winner of CIPHEX West’s New Product Gallery/Most Innovative Product Competition in the Air Conditioning, Refrigeration category.

The Design Envelope PSPC was selected from more than 60 entries by an independent jury that judged the products on meeting at least two of the following criteria:

Read More

Topics: Design Envelope, CIPHEX, In The Media, Parallel Sensorless Pump Controller

Parallel Sensorless Pump Controller launched

Posted by Armstrong Fluid Technology on Feb 3, 2014 11:48:02 AM

As seen on WorldPumps.com - February 3, 2014

Armstrong Fluid Technology unveils latest development.

The new parallel sensorless pump controller by Armstrong Fluid Technology (AFT) coordinates the operation of up to four Armstrong variable speed pumps to offer what the company claims is superior energy efficiency at a reduced first installed cost.

Read More

Topics: Design Envelope, Energy Efficient, Parrallel Sensorless Pump Controller, Sustainability, worldpumps.com, HVAC, Parallel Sensorless Pump Controller

Parallel Sensorless Pump Controller

Posted by Armstrong Fluid Technology on Sep 30, 2013 11:54:12 AM

As seen in Air Conditioning, Heating & Refrigeration NEWS, September 30, 2013

The Parallel Sensorless Pump Controller is an add-on control device that coordinates the output of multiple pumping units in a parallel configuration to achieve significant energy savings. Featuring advanced sensorless technology, the pump controller controls up to four of the manufacturer’s Design Envelope pumping units and delivers energy efficiency, along with reduced installation costs. The monitoring and instruction provided by a parallel sensorless pump controller can coordinate operations to achieve even greater energy savings. According to the manufacturer, when used in combination with its Design Envelope pumps, the Parallel Sensorless Pump Controller can help building owners significantly reduce their energy costs and achieve much greater efficiency throughout the system’s life cycle.

Read More

Topics: Magazine, Parrallel Sensorless Pump Controller, AHR News, Parallel Sensorless Pump Controller

Armstrong Launches Parallel Sensorless Technology

Posted by Armstrong Fluid Technology on Jun 26, 2013 3:09:21 PM

As seen on Heating Help - June 26, 2013

Armstrong Fluid Technology has announced the global launch of its Parallel Sensorless technology with the introduction of the Parallel Sensorless Pump Controller. The new Parallel Sensorless Pump Controller is an innovative add-on control device that coordinates the output of multiple pumping units in a parallel configuration to achieve significant energy savings.

Featuring advanced sensorless technology, the Parallel Sensorless Pump Controller controls up to four Armstrong Design Envelope pumping units and delivers superior energy efficiency, along with reduced first installed system cost. The monitoring and instruction provided by a parallel sensorless pump controller can coordinate operations to achieve even greater energy savings.

Read More

Topics: Armstrong Fluid Technology, Design Envelope, Energy Efficient, In The Media, Parallel Sensorless Pump Controller

Never miss a thing!

Be the first to get notified

Sign up for our blog notifications and you will be one of the first to know when there is new content. If you want to be in the know, sign up now.

Sign up for notifications now

Recent Posts

Posts by Topic

see all