Armstrong In The Media Blog

Armstrong Unveils Expanded Range of Three-speed Circulators

Written by Armstrong Fluid Technology | Feb 18, 2015 9:11:42 AM

As seen on healthcarefacilitiestoday.com - August 29, 2014

TORONTO - Armstrong Fluid Technology has announced the expansion of its Astro wet-rotor circulator offering with the introduction of the Astro 2 Series. Featuring four new sizes, the Astro 2 Series now offers flange-to-flange and bolt-to-bolt compatibility with 100% of competing models in terms of performance.

Designed for fast and convenient installation and years of trouble-free operation, the new models also address a broader range of applications. Key features include: three field-selectable operating speeds, double the head and triple the flow, a plug-in terminal strip to save time on installation, e-coating on the inside of the cast iron volutes to provide enhanced corrosion protection, pre-installed high-flow check valve and availability in cast iron, stainless steel and lead-free bronze.

In addition, Armstrong has announced an industry-leading five-year warranty on both the Astro and Compass Circulators. Commenting on the company’s commitment to a five-year warranty, Rod Hightower, Armstrong’s Commercial Director, US stated, "The five-year warranty is a reflection of the quality and reliability built into these products."

 

Also seen on: