As seen in Air Conditioning, Heating & Refrigeration NEWS, September 30, 2013
The Parallel Sensorless Pump Controller is an add-on control device that coordinates the output of multiple pumping units in a parallel configuration to achieve significant energy savings. Featuring advanced sensorless technology, the pump controller controls up to four of the manufacturer’s Design Envelope pumping units and delivers energy efficiency, along with reduced installation costs. The monitoring and instruction provided by a parallel sensorless pump controller can coordinate operations to achieve even greater energy savings. According to the manufacturer, when used in combination with its Design Envelope pumps, the Parallel Sensorless Pump Controller can help building owners significantly reduce their energy costs and achieve much greater efficiency throughout the system’s life cycle.
Also Seen On: