As Seen on empoweringpumps.com – November 11, 2017
Beyond the issue of ambient air temperature, the project presented a number of challenges that would affect the solution design. Maintenance and Production managers had determined that the cooling system would be needed by May, before the onset of the hot summer weather. That provided only a seven month window for design, fabrication, installation and commissioning. Additionally, because CKNA operates as a Tier 1 supplier to the automotive industry, they could not allow any interruptions to the production process. Floor space in the facility is maximized for production, so there was no available space to add equipment. The new system had to be provided as a prefabricated remote chilled water plant complete with an enclosure. Lastly, the electrical power available was limited by the size of an existing transformer. The installed solution would have to be energy efficient, and at the same time be capable of delivering 2000-tons of cooling.
Ultimately the many challenges of the project were addressed through a phased implementation, with 1000 tons of cooling targeting the hottest plant areas immediately, and then an additional 1000 tons, to address the remainder of the plant to be delivered at a later date.
Designed, assembled and tested in a controlled ISO 14000 factory environment, the Armstrong Chilled-Water Integrated Plant Package combines all the equipment needed to deliver chilled water in large buildings while maintaining superior energy efficiency. Armstrong product solutions built into this packaged system for CKNA included:
• IPC-11550
• Chilled Water Pumps
• Condenser Water Pumps
• Suction Guides
• Flo-Trex Valves
• Vortex Air Separator
• Expansion Tank
• Design Envelope 4300 Vertical In-Line Pumps
The project was a great success, with the completed system delivered to the site on time, with no cost overruns. The system was delivered to site as a complete package. Operating efficiency ranges between 0.49 kw/ton and 0.72 kw/ton, depending on the system load. Annual average is 0.65 kw/ton.
The setting of the chiller plant and cooling tower was completed in less than 3 days and complete system installation was completed in less than 4 weeks. Air temperatures in the plant dropped and remained at a much more comfortable level. There were no disruptions to plant operations, and the installed system is guaranteed to work within the stated restrictions for power usage. Lastly, the choice of a high-efficiency system means that operating costs are kept to a minimum.
By the end of August, managers were able to identify a number of direct and indirect benefits of the project, including increased employee productivity, improved staff retention and improvements in manufacturing quality indicators.
Request an Energy Audit to learn where energy savings can be found in your building.