The mining industry has entered a decisive decade – with 2030 looming as a critical interim milestone for reaching vital carbon and water reduction targets.
The challenge is that – despite ambitious and encouraging target setting – the execution remains uneven. The industry has moved beyond the need to define its sustainability ambitions, and is now facing the difficulties of operationalising these expectations. The key lies in embedding sustainability into the core mechanics of how mines function, rather than treating it as an overlay.
Much of the public narrative around decarbonisation in mining has focused on highly visible interventions: renewable energy installations, electrified haul fleets and hydrogen-powered equipment. These are undeniably critical. However, they represent only part of the solution.
Beneath the surface lies a complex network of energy-intensive systems, including fluid handling, dewatering, slurry transport and process water circulation. These functions collectively account for a substantial share of operational energy use. It is within these systems that some of the most immediate and cost-effective decarbonisation gains can be realised.
Mining operations are, at their core, large-scale energy conversion systems. Moving rock, water and slurry require continuous power input, often under variable and harsh conditions. Inefficiencies in these systems – resulting from issues like oversized equipment, throttled flows and poorly matched duty cycles – translate directly into wasted energy and elevated emissions. In most cases, these inefficiencies are not visible at a headline level, yet they persist across decades of operation, compounding both cost and environmental impact.
Addressing the challenges of what could be called ‘hidden energy’ requires a shift in perspective – from component-level optimisation to system-level thinking. High-efficiency motor technologies, for instance, can deliver significant gains, particularly when combined with variable speed drives (VSDs) that align energy consumption with real-time demand. Rather than operating at fixed speeds and dissipating excess energy through throttling, systems can dynamically adjust output, reducing both power consumption and mechanical stress.
Equally important is the integration of intelligent control systems that optimise performance across entire networks. Advanced pumping systems, when paired with real-time monitoring and automated flow control, can respond to changing process conditions with precision. This not only reduces energy waste but also extends asset life, lowers maintenance requirements and improves overall reliability. Evidence suggests that such interventions can reduce energy consumption in fluid systems by 30-40%, while delivering rapid return on investment.
With mining being so water-intensive, water stewardship presents a parallel – and increasingly urgent – dimension of the net zero equation. In many regions, water scarcity is becoming a defining operational constraint for new and existing mining operations. The shift toward net zero water is therefore not simply an environmental imperative but a business-critical requirement.
Here, too, operational technologies play a pivotal role. Closed-loop water systems, which prioritise recycling and reuse over continuous withdrawal, are gaining traction across the industry. By integrating high-efficiency pumping, filtration and treatment processes, for instance, mines can significantly reduce freshwater intake while maintaining process integrity. In some cases, water reuse rates of 50-80% are achievable, dramatically lowering both environmental impact and operational risk.
Real-time monitoring is central to this transformation. Intelligent water management systems, equipped with sensors and telemetry, provide continuous visibility into flow rates, pressure, quality and storage levels. This enables proactive decision-making that prevents over-pumping, detects leaks and optimises distribution across the site. The result is a more resilient and efficient water system, aligned with sustainability targets and operational demands.
Digitalisation is the connective tissue that binds these advances together. The integration of Internet of Things (IoT) technologies and artificial intelligence (AI) is fundamentally reshaping how mining systems are managed. Historically, operations have been reactive – simply responding to failures as they occur. Today, predictive models can anticipate issues before they escalate, enabling targeted maintenance and reducing unplanned downtime.
Predictive maintenance, driven by continuous data analysis, allows operators to identify patterns of wear and performance degradation. This not only improves equipment reliability but also ensures that systems operate at optimal efficiency throughout their lifecycle. Automated control systems further enhance this capability, adjusting parameters in real time to maintain optimal performance under varying conditions.
The implications for energy use and emissions are significant. Reduced downtime means fewer energy-intensive restarts, while optimised performance means less wasted power. Also, extended asset life means lower embodied carbon in replacement equipment. Collectively, these gains contribute to a more sustainable and cost-effective operation.
It is important to recognise, though, that these operational improvements are not a substitute for large-scale energy transition initiatives; rather, they are an enabler. Electrification of mining fleets, for example, delivers maximum benefit only when supported by efficient underlying systems. An electric haul truck powered by renewable energy still depends on a network of pumps, conveyors and processing equipment. If these systems are inefficient, they dilute the overall impact of electrification.
Similarly, the integration of renewable energy into mining operations introduces variability in power supply. Intelligent systems that can adapt to fluctuating energy availability – by modulating demand in response to supply – become essential. In this context, system efficiency is not merely about reducing consumption, but about enhancing flexibility and resilience.
The pathway to net zero in mining is therefore inherently multi-dimensional. It requires simultaneous progress across energy, water and digital domains, underpinned by a commitment to operational excellence. Companies that focus exclusively on headline initiatives risk overlooking the cumulative impact of everyday inefficiencies. Conversely, those that prioritise system-level optimisation can unlock immediate gains while building a foundation for long-term transformation.
Looking ahead, the next phase of decarbonisation will be defined by integration. The boundaries between energy systems, water systems and digital platforms will continue to blur, creating opportunities for holistic optimisation. For example, integrated control platforms could coordinate water management and energy consumption in real time, aligning pumping schedules with renewable energy availability. Models driven by artificial intelligence could optimise entire process chains – to balance throughput, energy use and water consumption.
This level of integration demands an operational mindset that views sustainability not as a constraint, but as a driver of innovation and efficiency. It also requires collaboration across disciplines, bringing together expertise in engineering, data science and environmental management.
Ultimately, mining companies who are most successful in this transition will be those that recognise that net zero is not achieved through isolated interventions, but through the cumulative effect of thousands of operational decisions.
By embedding efficiency into the fabric of their operations – across fluid systems, water management and digital infrastructure – they can move beyond aspiration to execution. This will position them to meet their net zero carbon and net zero water targets, while also becoming more resilient, competitive and sustainable.
By Divyanshu Shrivastava, Global Product Manager – Industrial Fluids at Armstrong Industrial, a division of Armstrong Fluid Technology
As Seen On: at-minerals.com June 16, 2026