Armstrong In The Media Blog

Chiller plant control solution

Written by Armstrong Fluid Technology | Jan 24, 2014 11:42:47 AM

As seen on csemag.com - January 24, 2014

Armstrong OPTI-VISOR controls the key components of a chiller plant, providing the optimal operating settings for equipment such as water-cooled variable speed chillers, variable flow cooling towers, and variable speed pumps on the chilled water and tower water circuits. Armstrong OPTI-VISOR is a relational control solution for the operation of an all-variable-speed chiller plant. OPTI-VISOR is an excellent solution for retrofit in buildings with water-cooled chiller plants, including those less than five years old, but is also suitable for new construction applications involving variable-primary flow chiller plants that have advanced building automation systems (BAS).

 OPTI-VISOR is designed for retrofit in buildings with water cooled chiller plants, including those less than five years old, but is also suitable for new construction applications involving variable-primary flow chiller plants that have advanced BAS.