As Seen on heatinghelp.com – August 24, 2017
The first Solution Outline entitled Intelligent Variable Speed Pumps details how intelligent variable speed pumps with Sensorless technology can provide HVAC systems with the lowest life cost by consuming only the energy required. The 12-page document features detailed charts, graphs and explanations of how HVAC professionals can achieve the highest value pumping system for their individual installations.
The second Solutions Outline (Tango Intelligent Variable Speed Pump) expands on the first by explaining how Tango Pumps with built-in Parallel Sensorless Pump Control can further reduce the first installed costs as well as lifetime costs by more than 30% compared to traditional approaches. The six-page document also uses detailed charts and graphs to illustrate how Design Envelope Tango Pumps can help building owners cut their energy costs while saving up to 75% of mechanical room space.
Both Solutions Outlines are available free-of-charge at http://armstrongfluidtechnology.com/~/media/documents/sales-and-marketing/solution-outlines/100-11_designenvelope_brochure.pdf?la=en and http://armstrongfluidtechnology.com/~/media/documents/sales-and-marketing/solution-outlines/100-20_designenvelope_tango_solutionoutline.pdf?la=en.
Also seen in: