Armstrong In The Media

Armstrong Unveils New End Suction Pumps that Eliminate Inertia Base

Posted by Armstrong Fluid Technology on Mar 18, 2025, 7:59:35 AM

As Seen On: empoweringpumps.com March 6, 2025

Provide Significant Cost & Energy Savings

4200H_6 ES Medium Pump _Standard - 30-30 L - With Cover

Armstrong Fluid Technology has introduced three larger sizes of Design Envelope End Suction Pumps, with Permanent Magnet motors up to 50hp that deliver impressive energy savings and eliminate the need for an inertia base.

“Because the new End Suction Pumps don’t require an inertia base, and Design Envelope technology eliminates the need for differential pressure sensors and flow meters, installation costs can be reduced by up to $5,000 per pump” said Zeljko Terzic, Offering Manager, Pumps. “Also, because of the factory-aligned rigid coupling, there is no need for coupling realignment during the installation process. This reduces installation time and related labor costs.”

The new End Suction Pumps also feature Design Envelope technology, with integrated intelligent controls, that can save up to 65% in energy over comparable traditional constant-speed or variable frequency operated pump installations.

Also Seen On:

 

Topics: Sustainability, In The Media, End-Suction Pumps, Energy Efficiency, Design Envelope pumps

Never miss a thing!

Be the first to get notified

Sign up for our blog notifications and you will be one of the first to know when there is new content. If you want to be in the know, sign up now.

Sign up for notifications now

Recent Posts

Posts by Topic

see all