Armstrong In The Media Blog

Armstrong unveils improved Astro 2 hot water recirculation systems

Written by Armstrong Fluid Technology | Feb 3, 2016 7:47:16 AM

As Seen on Healthcare Facilities Today - February 2, 2016

Armstrong Fluid Technology has introduced new versions of the popular Astro 2 Hot Water Recirculation (HWR) pumps.  A hot water recirculation system can save a typical family over 12,000 gallons of water per year by eliminating the waste of water that occurs when occupants open a hot water faucet and have to wait for hot water to reach the fixture.

Astro 2 HWR circulators are suitable for use in a 3-pipe installation with a dedicated return. The Astro Express 2 System includes the innovative Astro Express LF Valve and is designed for use in a standard residential 2-pipe installation.

Key enhancements offered in the new version of Astro 2 circulators include:

• Larger, easier-to-service electrical enclosure includes an integrated timer assembly

• Timer Accessory Kit that can be used to upgrade earlier version Astro 2 circulators

• New Timer Accessory Kit that can be used to upgrade new generation Astro 2 circulators

• Easier field assembly of timers reduces installation time

• Industry-leading five year warranty

Astro 2 HWR circulators are available in both stainless steel and bronze versions, with either NPSM Union or ‘sweat’ connections.

“In addition to offering customers more sustainable solutions, the new Astro 2 HWR helps contractors and homeowners with easier installation and an industry-leading warranty.” said Andy Januszewski, Armstrong Marketing Manager.

Also seen in: