Armstrong In The Media

Armstrong Launches New Models of Compass R Circulators with Dry Rotor Design

Posted by Armstrong Fluid Technology on Aug 21, 2025, 7:26:02 AM
As Seen On: impeller.net August 11, 2025
Armstrong Launches New Models of Compass R Circulators with Dry Rotor Design

Armstrong Fluid Technology has introduced two new sizes, 40-85 and 60-50, of Design Envelope Compass R circulators. The Compass R is an energy-efficient variable speed dry-rotor circulator.

Designed to replace existing fixed-speed circulators, Compass R can be considered a universal energy upgrade for circulators in its capacity range and installation profile. Customers can purchase Compass R circulators to serve applications requiring up to 60 feet of head.

Commenting on the release of the two new models, Tanvir Rahman, Offering Manager, Standard Building Products, noted: “The Compass R offers an industry-leading feature set including a fully repairable dry rotor design, easy access for repairs changes and embedded Design Envelope variable speed technology. The new models will make these features available to more customers and a wider range of applications”

The new Compass R features include:

  • Permanent magnet motor with Design Envelope variable speed technology
  • Posi-start Technology ensures smooth start-up and pump protection
  • Bolt-for-bolt compatibility with wide range of installed circulators
  • Quick-release clamp that makes repairs easy
  • Reduced carbon footprint
  • Easy terminal block access
  • Optimized hydraulics with high-efficiency dry rotor design
  • Multiple control options, including Auto mode, simplify selection and commissioning

Also Seen On:

Never miss a thing!

Be the first to get notified

Sign up for our blog notifications and you will be one of the first to know when there is new content. If you want to be in the know, sign up now.

Sign up for notifications now

Recent Posts

Posts by Topic

see all