As seen on hvacinformed.com 23rd January, 2024
Driven by the demand for low-cost energy and the growing number of organizations committing to Net-Zero targets, the global market for District Heating and Cooling Systems market is expected to grow to over $745 billion by 2032.
Read More
Topics:
District Energy,
HVAC,
In The Media,
District Heating
April 22nd is designated as Earth Day. We spend the day (and perhaps a few days on either side) thinking more carefully about the environment and our impact on it. We make commitments around the many ways the years ahead will be different. How we can change. How we can consume less. How we can be more responsible. How we can reduce our carbon footprint, and purchase carbon credits to erase the rest.
Read More
Topics:
Environmental Goals,
Earth Day
As seen on impeller.net January 24, 2024
Armstrong Fluid Technology has introduced an expanded range of Design Envelope Permanent Magnet pumps that are engineered to deliver 35-65% reduction in energy consumption compared to conventional integrated pumps with induction motors.
Available in mid-February with motors up to 60hp, these Design Envelope Permanent Magnet operate at NEMA Ultra-Premium efficiency levels that exceed the targets set by the US Department of Energy and the NRCan Office of Energy Efficiency.
Read More
Topics:
Design Envelope,
In The Media,
Permanent Magnet Motors,
Design Envelope Technology
Armstrong Fluid Technology has announced the launch of Fire Manager, a cloud-based service that enables Active Performance Management in its industry-leading Design Envelope Fire Pumps.
The innovative new service proactively tracks and manages pump performance and provides early diagnostic warnings and timely automated reports that help customers make informed decisions and take immediate action to deliver the most efficient and safest
fire safety
system performance.
Read More
Topics:
In The Media,
Fire Safety,
Fire Pump Manager
Jacob Wolfe, a seasoned professional with extensive experience in the data center industry, has been appointed as the Regional Manager for Data Center Sales & Business Development in the Americas region by Armstrong Fluid Technology. In his new role, Wolfe will be responsible for driving business development initiatives and implementing sales strategies to enhance Armstrong’s presence in the data center market.
Read More
Topics:
Data Center
Pumps that are designed and approved for fire suppression systems can be grouped into four major categories based on configuration.
Read More
Topics:
Design Envelope,
Fire Pumps
Design Envelope Fire pumps are designed, assembled, and tested to meet the code requirements of a Self-Regulating Variable Speed Fire Pump Unit, as described in NFPA 20 – 2019 edition. Design Envelope Fire pumps are factory-built, integrated fire pumps consisting of a Vertical In-Line pump, driver, and variable speed control unit. They’re configured to maintain a set pressure until the maximum power draw is reached, while modulating pump speed to control to meet limits on pressure or suction.
Read More
Topics:
Design Envelope,
Fire Pumps,
Design Envelope Fire pump unit
Horizontal Split Case Fire Pump
These pumps use a between-the-bearings design, which means that the impeller is supported by bearings on both sides. This design provides more support for the impeller and enables it to rotate more efficiently under stress. HSC pumps place the suction and discharge nozzles (flanges) in the bottom half of the casing, on opposite sides. The impeller shaft is positioned slightly above the flanges. This sturdy but simple design is particularly suitable for higher flow applications, because it reduces thrust loads on the pump shaft and allows for operation over a broad range of flows.
Read More
Topics:
Fire Pumps,
Pumps
Since its founding in 1934 the company has expanded from the challenges of the Great Depression to become a leader in its field.
TORONTO, CAN —
Armstrong Fluid Technology
marked its 90th anniversary this April, celebrating a significant milestone of longevity and innovation in the fluid-flow systems industry. Since its founding in Toronto, Canada, in 1934 by
Samuel
Allan Armstrong, the company has expanded from the challenges of the Great Depression to become a leader in its field. Today, Armstrong operates eight manufacturing facilities across four continents, showcasing its global reach and commitment to excellence in design, engineering, and manufacturing.
Read More
Topics:
In The Media,
CEO
Where do Circuit Balancing Valves (CBVs) fit in a hydronic system?
CBVs should be included in every branch of a hydronic system. For many applications such as boilers, chillers and heat pumps, they are needed to ensure balanced or equalized flow of water to all parts of a building and, as required by heating or cooling loads, across all branches of a system.
Read More
Topics:
Hydronics,
In The Media,
CBV