As Seen On: empoweringpumps.com March 2, 2021
District heating scheme in Blackburn Meadows, Sheffield, generates heat and energy from waste wood with the help of Armstrong Fluid Technology [Case Study]
Topics: In The Media, Variable speed pumps, District Heating, IPS 4000 Pump Controller
Savings Delivered Between Trains from Variable Speed Operation [Case Study]
As Seen On : empoweringpumps.com - February 8, 2022
Background
Anacostia is a commuter train station in Washington, D.C. on the Washington Metropolitan Area Transit Authority (wmata) Metrorail Green Line. The station serves Metrorail and Metrobus passengers traveling to and from the Anacostia neighborhood in Southeast Washington.
Topics: Design Envelope, ifms, In The Media, Variable speed pumps, Energy Efficiency
As Seen on cdn.coverstand.com - May 2019
Topics: In The Media, Pump Manager, Variable speed pumps
HVAC Pumping Efficiency: Variable Speed Saves Energy in Constant Flow Systems
As seen on empoweringpumps – March 07, 2017
Author: Brent Ross, Director, Armstrong Fluid Technology
There is a misconception in the HVAC marketplace that needs to be addressed. Unfortunately, many people believe they only need variable speed when they have variable flow applications. This might be because the recently updated ASHRAE 90.1 2016 rules essentially do not require variable speed in constant flow applications. ASHRAE 90.1 is a minimum requirement, and if there are ways to save more energy than what is required as a “minimum”, we should absolutely be trying to save more energy than what is minimally required. Using variable speed in constant flow systems, the HVAC industry has an opportunity to save an average of 15 to 16% energy and sometimes over 50% and more.
Topics: Energy Saving, In The Media, Variable speed pumps
A Systems Approach Maximizes Energy Savings Potential
As seen on pumpsandsystems.com – December 2016
Variable speed pumps in a recreation complex save a college thousands of dollars per year in energy costs.
by Brent Ross
Pumping systems consume a significant portion of global electrical energy, accounting for nearly 20 percent of the energy used by electric motors and 25 to 50 percent of the total electrical usage in certain industrial facilities.
Ironically, pumping systems are rarely included in energy-efficiency calculations, even though pumps present such energy-savings potential. One could argue that mentioning “motor” or “variable speed drive” (VSD) is sufficient because these components indicate the greatest energy-savings opportunity in a pumping system.
Topics: Energy Saving, In The Media, Variable speed pumps
As Seen on empoweringpumps.com – December 11, 2016.
Indo-MIM is a manufacturer and supplier of metal injection molding parts located in Bangalore India. Founded in 1997, Indo-MIM is a world leader in metal injection molding, serving customers such as Honeywell, TRW and Bosch. The two major Indo-MIM facilities are located at Hoskote and Doddaballapur in India.
Topics: Energy Efficient, Case Study, In The Media, Variable speed pumps
Armstrong Variable Speed Pumps Slash Energy Consumption of Birmingham Office Block
As seen on impeller.net - March 04, 2016
Variable speed pumps from Armstrong Fluid Technology are reducing energy consumption at The Axis – a major commercial building in the centre of Birmingham. Employing demand-based control technology, the Armstrong pumps will significantly reduce utility bills and improve the building’s environmental performance.
Topics: In The Media, Variable speed pumps