Armstrong In The Media

Pump Types

Posted by Armstrong Fluid Technology on Nov 7, 2023 4:20:12 PM

A Review of Pump Types for HVAC Systems

Pumps can be grouped according to the method of displacement, the direction of fluid flow, orientation, and control capabilities. Major types of pumps include positive-displacement pumps, centrifugal pumps, and axial flow pumps.

Read More

Topics: Commercial Pumps, Fire Pumps, HVAC System, In The Media, Tango, Vertical, Twin Pumps, Fire Safety, Pumps, Variable Speed Drives

Armstrong Fluid Technology Announces New Fire Pump Parts Kits

Posted by Armstrong Fluid Technology on Dec 7, 2022 6:26:38 AM

As Seen on: heatinghelp.com, November 29, 2022

 

Armstrong Fluid Technology has announced the availability of new Parts Kits for Fire pumps. Consisting of engineered combinations of Armstrong genuine parts, the Parts Kits include all the replacement parts and related hardware required to complete the service and maintenance tasks that fire pumps require.

Read More

Topics: Fire Pumps, In The Media, Replacement Parts, Parts Kits

Armstrong Introduces the Self-Regulating Variable Speed Fire Pump

Posted by Armstrong Fluid Technology on Jun 24, 2019 5:58:51 AM

As Seen on news.thomasnet.com - June 19, 2019

Meets NFPA-20 (2019 Edition), Section 4.8 Standards

Toronto, June 18, 2019 – Armstrong Fluid Technology has unveiled its industry-leading, self-regulating variable speed fire pump which, in addition to new safety benefits, also holds the distinction of being the first fire pump to meet NFPA-20 (2019 Edition), Section 4.8 standards. 

“The new Design Envelope Fire Pump will provide safe, reliable performance in fire suppression systems, along with complete transparency into the operation of the pump. The Design Envelope Fire Pump also makes fire suppression systems that require a variable speed approach more affordable for contractors and building owners, as it enables a more cost-effective design for the fire sprinkler system.” said Steven Baird, Marketing Manager – Fire Products at Armstrong.

Read More

Topics: Fire Pumps, In The Media, NFPA, Variable Speed Fire Pump, NFPA-20

Smarter fire suppression systems take center stage at NFPA

Posted by Armstrong Fluid Technology on Jun 24, 2019 4:04:13 AM

As Seen on modernequipmentmanufacturer.com - June 19, 2019

This week marks the beginning of the annual National Fire Protection Association (NFPA) Conference and Expo. This means that the world’s leading fire safety experts – as well as the most innovative fire protection solutions providers – have descended on San Antonio to discuss fire codes and regulations, share best practices and discuss the trends and technologies that are helping to make people safer at home and on the job.

Read More

Topics: Fire, Fire Pumps, In The Media, NFPA, NFPA Conference

Energy-efficient fire pumps from Armstrong Fluid Technology

Posted by Armstrong Fluid Technology on May 31, 2018 10:10:46 AM

As Seen on pmengineer.com – May 22, 2018

Armstrong Fluid Technology updates its Fireset Horizontal Split Case Pump line with two new models: a 5x4x10NF fire pump for installs requiring 500 gpm at pressures from 55 to 167 psi and a 8x6x15 option for applications requiring flows between 1,500 and 2,000 gpm at pressures from 54 to 168 psi. The new Fireset HSC pumps have double suction design for operating efficiency and high-flow performance, right- or left-hand suction configuration with electric-driven pumps for adapting to mechanical room piping arrangements and a compact design for easy installation and maintenance.

Read More

Topics: Fire Pumps, In The Media, Fireset, HSC

Armstrong launches high performance fire pump models

Posted by Armstrong Fluid Technology on Feb 6, 2018 9:09:08 AM

As Seen on arabianindustry.com – January 23, 2018

Armstrong Firesetpumps feature a double suction design for superior levels of operating performance.

Armstrong Fluid Technology will be debuting a new line of high performance fire pump models at Intersec 2018 in Dubai. 

The Armstrong Fireset Horizontal Split Case (HSC) fire pumps offer superior flow performance and incorporate features for ease of installation and maintenance.

Read More

Topics: Fire Pumps, In The Media

New Fire Pump Sizes

Posted by Armstrong Fluid Technology on Nov 24, 2017 2:05:28 AM



Armstrong has expanded its 4600F Horizontal Split Case (HSC) pump line with two new technologically advanced models.

The new 5x4x17F and 6x5x12F pumps are ideal for installations that require between 500 and 1,000 USgpm.

Read More

Topics: Fire Pumps, HSC Firepak, In The Media

Armstrong Fluid Technology Introduces Two New HSC Energy-efficient Fire Pump Models

Posted by Armstrong Fluid Technology on Jun 5, 2017 10:27:09 AM

As seen on heatinghelp.com – May 25, 2017 

The two new Fireset™ Horizontal Split Case (HSC) pump models are compatible with Armstrong’s HSC Firepak, a completely integrated fire pump solution that provides both designers and contractors with a unique set of advantages. The innovative “Plug and Play” design allows fast and easy installation.

 

Armstrong Fluid Technology has enhanced its Fireset™ Horizontal Split Case (HSC) pump line with two new technologically advanced models.

The two new Fireset™ Horizontal Split Case (HSC) pump models are compatible with Armstrong’s HSC Firepak, a completely integrated fire pump solution that provides

Read More

Topics: Fire Pumps, HSC Firepak, In The Media

Armstrong Fluid Technology Announces New Size of HSC Firepak™ for 300 psi

Posted by Armstrong Fluid Technology on Jun 21, 2016 3:37:39 AM

As seen on HeatingHelp.com – June 13, 2016

TORONTO — Armstrong Fluid Technology has introduced its enhanced HSC Firepak™, a completely integrated fire pump solution that delivers a unique set of advantages to both designers and contractors.

Featuring a compact design for fast and easy installation, Armstrong’s “Plug and Leave” design provides fire safety professionals with a complete fire pump solution that offers:

Read More

Topics: Fire Pumps, HSC Firepak, In The Media

Fire Sprinkler Systems

Posted by Armstrong Fluid Technology on May 24, 2016 6:30:36 AM

As seen on reevesjournal.com– May 12, 2016

from Steven Baird

Required or optional, contractors would do well to know about these safety systems

Read More

Topics: Fire, Fire Pumps, In The Media

Never miss a thing!

Be the first to get notified

Sign up for our blog notifications and you will be one of the first to know when there is new content. If you want to be in the know, sign up now.

Sign up for notifications now

Recent Posts

Posts by Topic

see all