Armstrong In The Media

Fire Pump Market Global Industry Analysis, size, share and Forecast 2016-2026

Posted by Armstrong Fluid Technology on Nov 7, 2016 4:19:30 AM

As Seen on mynewsdesk.com – October 11, 2016.

Rapid industrialization is expected to positively impact the demand for fire pump in the near future. A fire pump is a part of water supply of fire sprinkler systems is run by using electric, diesel or steam. The fire pump is connected to either a static water source (tank, lake, and reservoir) or an underground water supply piping. Generally, it is connected with the public underground water supply pipe or any static water source such as tank, reservoir, and lake. The fire pump machine offers high pressure water flow to the fire sprinkler systems. The fire pump starts working when the fire sprinkler’s pressure drops below a certain set point (threshold). The number of fire pump should be installed depending on the occupancy hazard and the specific fire installation standard. Most of the fire pumps are listed, tested, certified by the accredited laboratories and authorized institutions. According to various research reports, the fire pumps market is anticipated to increase at a significant rate over the forecast period.

Read More

Topics: Armstrong Fluid Technology, Fire Pump Market, In The Media

Never miss a thing!

Be the first to get notified

Sign up for our blog notifications and you will be one of the first to know when there is new content. If you want to be in the know, sign up now.

Sign up for notifications now

Recent Posts

Posts by Topic

see all