Armstrong In The Media

Armstrong Unveils New Line of High Performance Design Envelope End Suction Pumps

Posted by Armstrong Fluid Technology on Feb 6, 2018 7:05:46 AM

Unique Vibration Isolation Technology Further Extends Installed Cost Savings and Customer Options.

Toronto, January 22, 2018 – Armstrong Fluid Technology has announced the availability of a new line of high performance Design Envelope End-Suction pumps in the 1 to 10 hp range. These new offerings reflect a completely new design featuring improved hydraulics and Armstrong intelligent motor technology. The new offerings also feature Armstrong’s unique vibration isolation technology, which can reduce installed costs by as much as $2000 by eliminating the need to add an inertia base on installation.

Read More

Topics: Design Envelope, In The Media, End-Suction Pumps

Armstrong Holds Press Conference at AHR Expo

Posted by Armstrong Fluid Technology on Feb 5, 2018 8:36:57 AM

As Seen on achrnews.com – January 22, 2018

Armstrong Fluid Technology held a press conference at its booth at the AHR Expo Monday announcing the availability of a new line of high performance Design Envelope End-Suction pumps in the 1 to 10 HP range.

“Last year was big year for us, we did two major introductions last year – our completely new 1-10 hp line,” said Neil Cooper, director, sales enablement, Armstrong Fluid Technology. “We’re still featuring the line you would have seen last year, featuring all the new elements of our next generation of offerings, and that’s the onboard controls, completely redesigned hydraulics, and most important, all the connectivity that goes with these. That’s wireless, wired, and traditional BACnet, no matter what you’re trying to connect these units to, it’s there.”

Read More

Topics: Design Envelope, In The Media, AHR2018, End-Suction Pumps

Never miss a thing!

Be the first to get notified

Sign up for our blog notifications and you will be one of the first to know when there is new content. If you want to be in the know, sign up now.

Sign up for notifications now

Recent Posts

Posts by Topic

see all