Armstrong In The Media

Armstrong unveils improved Astro 2 hot water recirculation systems

Posted by Armstrong Fluid Technology on Feb 3, 2016 2:47:16 AM

Astro2_HWRAs Seen on Healthcare Facilities Today - February 2, 2016

Armstrong Fluid Technology has introduced new versions of the popular Astro 2 Hot Water Recirculation (HWR) pumps.  A hot water recirculation system can save a typical family over 12,000 gallons of water per year by eliminating the waste of water that occurs when occupants open a hot water faucet and have to wait for hot water to reach the fixture.

Astro 2 HWR circulators are suitable for use in a 3-pipe installation with a dedicated return. The Astro Express 2 System includes the innovative Astro Express LF Valve and is designed for use in a standard residential 2-pipe installation.

Key enhancements offered in the new version of Astro 2 circulators include:

• Larger, easier-to-service electrical enclosure includes an integrated timer assembly

• Timer Accessory Kit that can be used to upgrade earlier version Astro 2 circulators

• New Timer Accessory Kit that can be used to upgrade new generation Astro 2 circulators

• Easier field assembly of timers reduces installation time

• Industry-leading five year warranty

Astro 2 HWR circulators are available in both stainless steel and bronze versions, with either NPSM Union or ‘sweat’ connections.

“In addition to offering customers more sustainable solutions, the new Astro 2 HWR helps contractors and homeowners with easier installation and an industry-leading warranty.” said Andy Januszewski, Armstrong Marketing Manager.

Also seen in:

 

Topics: Astro2, Circulator, In The Media

Never miss a thing!

Be the first to get notified

Sign up for our blog notifications and you will be one of the first to know when there is new content. If you want to be in the know, sign up now.

Sign up for notifications now

Recent Posts

Posts by Topic

see all