Armstrong In The Media

New Armstrong COMPASS R Represents the Next Technology Evolution for Circulators

Posted by Armstrong Fluid Technology on Mar 6, 2017 2:06:26 AM

As seen on empoweringpumps.com – April 12, 2017

 

Featuring Advanced Variable Speed Design and New ECM Motors

 

Armstrong Fluid Technology has announced the next technology evolution for circulators with the introduction of the COMPASS R. Featuring advanced variable speed Design Envelope technology, new high-efficiency Armstrong iECMTM motors, and quadratic pressure curves, the COMPASS R will minimize both energy costs and long-term operating costs for homeowners.


Other innovative features of the COMPASS R circulator include:

• High-efficiency dry rotor design
• Optimized hydraulics
• Replaceable mechanical seal
• Bolt-for-bolt connection compatibility with a range of installed 3-piece circulators
• Onboard control panel for easy selection of the appropriate operations mode and flow
• Release latch for easy adjustment of the display orientation and repairability
• Easy-to-access front-facing terminal block
• Large wiring chamber
• Complies with EEI<0.22

The COMPASS R offers multiple control options and an auto mode that adjusts the speed to match flow requirements. The new Armstrong circulator is available in .25 hp to 1.5 hp models with a maximum flow rate of 225 GPM and maximum head of 65 feet.

“Incorporating advanced Design Envelope technology into our circulators, coupled with the high efficiency iECM motors adds significant value through improved operating efficiency and sensorless, demand-based control,” said Andy Januszewski, Armstrong Marketing Manager.

Also seen in:

Topics: Compass R, Circulator, In The Media

Never miss a thing!

Be the first to get notified

Sign up for our blog notifications and you will be one of the first to know when there is new content. If you want to be in the know, sign up now.

Sign up for notifications now

Posts by Topic

see all