Armstrong In The Media

Achieving Greater Efficiency in Retrofits Using Parallel Sensorless Pump Control

Posted by Armstrong Fluid Technology on Jun 16, 2014 5:04:07 AM

As seen on empoweringpumps.com - June 16, 2014

25062014_1Parallel pumping is a common design in HVAC systems. To combine the advantages of parallel pumping with intelligent variable speed technology, Armstrong now offers Design Envelope Parallel Sensorless™ pump control. This new control technology can be added to any Design Envelope Vertical In-Line or dualARM pump, to provide advanced, variable flow, parallel pumping.

The Parallel Sensorless Pump Controller (PSPC) controls up to 4 Design Envelope pumps, adjusting speed for optimal energy efficiency and sequencing the units for even distribution of operating hours. The controller measures only 5″x7″, so it mounts conveniently on Design Envelope pumps.

The Armstrong PSPC Solution adds value to an HVAC system with features such as:

  • Advanced control to optimize up to four Design Envelope pumps
  • True best efficiency staging
  • Easy transfer of the PSPC from one pump to another

Armstrong is hosting a webinar to present and explain Parallel Sensorless Pump Control and outline the energy savings available. It will be held Friday June 27th at 11:00AM Eastern.

Register now to join in and learn more about the technology.

Topics: Armstrong Fluid Technology, Empowering Pumps

Never miss a thing!

Be the first to get notified

Sign up for our blog notifications and you will be one of the first to know when there is new content. If you want to be in the know, sign up now.

Sign up for notifications now

Recent Posts

Posts by Topic

see all