As seen on impeller.net January 24, 2024
Armstrong Fluid Technology has introduced an expanded range of Design Envelope Permanent Magnet pumps that are engineered to deliver 35-65% reduction in energy consumption compared to conventional integrated pumps with induction motors.
Available in mid-February with motors up to 60hp, these Design Envelope Permanent Magnet operate at NEMA Ultra-Premium efficiency levels that exceed the targets set by the US Department of Energy and the NRCan Office of Energy Efficiency.
Read More
Topics:
Design Envelope,
In The Media,
Permanent Magnet Motors,
Design Envelope Technology
Armstrong Fluid Technology has announced the launch of Fire Manager, a cloud-based service that enables Active Performance Management in its industry-leading Design Envelope Fire Pumps.
The innovative new service proactively tracks and manages pump performance and provides early diagnostic warnings and timely automated reports that help customers make informed decisions and take immediate action to deliver the most efficient and safest
fire safety
system performance.
Read More
Topics:
In The Media,
Fire Safety,
Fire Pump Manager
Pumps that are designed and approved for fire suppression systems can be grouped into four major categories based on configuration.
Read More
Topics:
Design Envelope,
Fire Pumps
Design Envelope Fire pumps are designed, assembled, and tested to meet the code requirements of a Self-Regulating Variable Speed Fire Pump Unit, as described in NFPA 20 – 2019 edition. Design Envelope Fire pumps are factory-built, integrated fire pumps consisting of a Vertical In-Line pump, driver, and variable speed control unit. They’re configured to maintain a set pressure until the maximum power draw is reached, while modulating pump speed to control to meet limits on pressure or suction.
Read More
Topics:
Design Envelope,
Fire Pumps,
Design Envelope Fire pump unit
Horizontal Split Case Fire Pump
These pumps use a between-the-bearings design, which means that the impeller is supported by bearings on both sides. This design provides more support for the impeller and enables it to rotate more efficiently under stress. HSC pumps place the suction and discharge nozzles (flanges) in the bottom half of the casing, on opposite sides. The impeller shaft is positioned slightly above the flanges. This sturdy but simple design is particularly suitable for higher flow applications, because it reduces thrust loads on the pump shaft and allows for operation over a broad range of flows.
Read More
Topics:
Fire Pumps,
Pumps
Since its founding in 1934 the company has expanded from the challenges of the Great Depression to become a leader in its field.
TORONTO, CAN —
Armstrong Fluid Technology
marked its 90th anniversary this April, celebrating a significant milestone of longevity and innovation in the fluid-flow systems industry. Since its founding in Toronto, Canada, in 1934 by
Samuel
Allan Armstrong, the company has expanded from the challenges of the Great Depression to become a leader in its field. Today, Armstrong operates eight manufacturing facilities across four continents, showcasing its global reach and commitment to excellence in design, engineering, and manufacturing.
Read More
Topics:
In The Media,
CEO
Where do Circuit Balancing Valves (CBVs) fit in a hydronic system?
CBVs should be included in every branch of a hydronic system. For many applications such as boilers, chillers and heat pumps, they are needed to ensure balanced or equalized flow of water to all parts of a building and, as required by heating or cooling loads, across all branches of a system.
Read More
Topics:
Hydronics,
In The Media,
CBV
As Seen On: technicalreviewmiddleeast.com January 22, 2024
Packaged chiller plant rooms within data centres cut installation time by up to 95%. (Image source: Adobe Stock)
Kevin Laidler, sales director for Middle East and Africa at Armstrong Fluid Technology, writes forTechnical Review Middle East, explaining how innovations in the HVAC sector can help data centres.
Read More
Topics:
Data Center,
HVAC,
HVAC System,
In The Media,
HVAC Installations
This condo tower (324 units on 13 floors) had completed a previous retrofit that unfortunately left the variable speed pumps operating in a fixed mode at low speed, so the HVAC system couldn’t cool the west-facing units in the summer.
Read More
Topics:
Energy Saving,
Energy Upgrade,
Energy - saving pumps,
In The Media
Central Memorial High School creates opportunities for 1100 students to focus on the arts, athletics or trades. In 2018, Armstrong worked with the Calgary board of Education to upgrade the hvac system for better efficiency and comfort.
Read More
Topics:
Energy,
Energy Upgrade,
Energy - saving pumps,
In The Media